How can we help you today?

What Are Level 1, Level 2, and Level 3 EV Charging?

EV charging is usually described in three levels. Level 1 uses a standard 120 V household outlet and is the slowest option.

Level 2 uses a 240 V circuit in home applications and is the most common choice for faster home charging. Schneider Charge is a Level 2 charger with up to 11.5 kW output, adding up to 44 miles of range per hour depending on the vehicle and conditions.

DC fast charging, sometimes called Level 3, is typically found at public charging sites and is designed for much faster charging during travel.

For more information about charging levels, please see Qmerit's blog at https://qmerit.com/blog/intro-to-level-1-and-level-2-ev-charging-at-home/

Schneider Electric Canada

Explore more
Range:
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Product:
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings