How can we help you today?

What is the CT protection accuracy class for the S33579 External Sensor for Source Ground-Return Protection?

Issue:
CT protection accuracy class

Product Line:
S33579 External Sensor for Source Ground-Return Protection

Resolution:
We do not provide accuracy for the sensor alone, but a global accuracy ( including CT + MDGF + micrologic measurement channel) : as per the user manual for ground fault is +/-10%. The frequency of use : 50/60Hz.