How can we help you today?

Can the Unity Momentum CPU be powered up without an IO base?

No. It is not possible to supply power to the 12 pin connector located under the CPU in order to make it functional. The CPU requires an IO base in order to complete the circuitry that will give it the 'PLC READY' which will allow communications and functionality.

This applies to 171CBU**as well as the older 171CCC** models.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors