How can we help you today?

Can the Schneider Home Power Mount cover frame be painted or decorated with stickers or decals?

No. The Power Mount cover frame is not designed to be painted, covered with stickers, or otherwise decorated.

The cover frame is made from LSR (Liquid Silicone Rubber), which serves several important functions:

  • Provides a high-quality aesthetic and soft-touch finish.
  • Helps absorb shocks and reduce noise when installing the HomeView.
  • Helps limit rotational force when adjusting the HomeView on the Wall Mount, reducing the risk of damage to the USB connectors.

Because of the material and its functional properties, applying paint, stickers, decals, or other surface treatments is not recommended. No specific paint type or surface preparation method is recommended for the cover frame.

Once the HomeView is installed, the cover frame is also mostly concealed, so its color has minimal visual impact on the finished installation.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings
  • Preference Center