Setup did not finish after I scanned the QR code to commission my X Series Matter Wi-Fi device. What should I do?
Perform a factory reset and repeat commissioning using the QR code, or pair manually using the 11-digit setup code. The code is on the QR sticker on the front of the device, on the yoke, or laser-marked on the side of the product.