Naše značky

Impact-Company-Logo-English Black-01-177x54

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How do I protect the project in my M580 PAC?
Issue:
Protecting the project in an M580 PAC


Product Line:
M580 PAC


Resolution:
The input %lr.m.c where r.m.c= rack.module.channel; can be parameterized to protect the internal application RAM and the memory
card as follows:
-  %lr.m.c set to 0: The internal application and the memory card are not protected.
-  %lr.m.c set to 1: The internal application and the memory card are protected.

*** This is not supported with the M580 Hot Standby controllers ***