Naše značky

Impact-Company-Logo-English Black-01-177x54

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Does Vijeo Designer v6.2 supports Windows 10?
Issue:
Is Vijeo Designer version 6.2 Windows 10 compatible?

Product Line:
HMI, Magelis, Vijeo Designer

Environment:
Windows 10

Cause:

Resolution:
Starting from Vijeo Designer 6.2 SP6, Windows 10 will be supported officially. All the documentation has been updated to reflect this in the Help menus and manuals.