Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Can an ATV320 be programmed to run an automatic preset speed in reverse?
Issue:
Needs to program the ATV320 to run a preset speed in reverse.

Product Line:
Altivar 320 drives

Resolution:
Yes you can program a digital input to be a preset speed and jumper that input terminal to the run reverse input terminal. This way, the run reverse and preset speed function will both go active simultaneously.  Note that the run forward command needs to be removed when giving the drive a run reverse command.

If the preset speeds function is already assigned for forward speeds, the same inputs can also be used in reverse. The presets speeds function simply provides a speed reference and is separate from the run forward or reverse commands. So preset inputs can be triggered in both forward and reverse.