Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How can I duplicate n-products in diagram in eDesign Small Building application
Issue: Duplicating n-products in diagram of eDesign small building application
Product Line: eDesign Small Building https://edesign-630.se.com/
Cause: Easy duplication of n-products in diagram
Resolution:
  1. Go to the Diagram tab in eDesign Small Building https://edesign-630.se.com/

  1. Click 3 dots on any of the Products, such as Group Feeder, Outgoer, Scheduling Management, Switch Disconnector, Additional protection, miscellaneous.
  2. Add multiple devices just by incrementing the counter numbers.


Note: This feature is available for the following functions:  Group Feeder, Outgoer, Scheduling Management, Additional Protection, miscellaneous.