Naše značky

Impact-Company-Logo-English Black-01-177x54

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Why the autorun option has no effect if it turned on ?
In certain contexts, using the M580 PLC in control Expert version 15.1 to 15.3, it happens that the PLC does not restart in RUN even though the "Autorun" option is validated.
Autorun option illustration
Illustration example, "autorun" option for BMEP582020

This problem only occurs when a configuration modification (addition/deletion of a module, a rack, etc.) is made and followed by an online build.

The only solution in this case is to do a "rebuild all" and transfer the application to the PLC.

This operating issue is corrected in version 16 of Control Expert.