Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Does EcoStruxure Control Expert support bit extraction of a DINT, DWORD and UDINT data type?

Issue:

Bit extraction of DINT, DWORD and UDINT data type in Ecostruxure Control Expert

Product Line:

EcoStruxure Control Expert

Resolution:

As of Control Expert V15.3, bit extraction of a DINT, DWORD and UDINT data type is allowed. Prier to this version it was not allowed.

image1