Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How do I perform the initial internal battery connection? | Back UPS PRO BX

Issue:

The Back UPS PRO BX model (BX850M/1000M/1350M/1500M) does not power on or begin charging when first connected.

Product Line:

Back UPS PRO BX

Environment

  • BX850M-LM60

  • BX1000M-LM60

  • BX1350M-LM60

  • BX1500M-LM60

Cause:

When purchasing a UPS from the Back UPS PRO BX family, it is necessary to perform the initial connection of the internal battery before operating the unit. If this step is skipped, the UPS will not function properly or begin charging its batteries.

Resolution:

To connect, disconnect, or replace the internal battery, follow the steps shown in the images below:

8 image

7 image