Issue:
For 115v input ATV12 drives, what should the UnS parameter be set at?
Product Line:
ATV12
Resolution:
If the Line voltage is less than the rated motor voltage, the rated motor voltage should
be set to the value of the line voltage, applied to the terminals.
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)“
Veröffentlicht für: Schneider Electric Deutschland