Are optional outdoor heat exchangers (OHE) available with the InRow ACRD?
Issue:
Are optional outdoor heat exchangers (OHE) available with the InRow ACRD?

Product line:
ACRD100, ACRD101, ACRD200, ACRD201

Environment:
Data Center Cooling

Cause:

Resolution:
APC has standard SKUs available for a limited set of outdoor condensers and fluid coolers. Additional OHEs may be configured and custom ordered with the help of Applications Engineering team. Standard lead times do not apply to these units.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: