What is the granularity of the PM600 series processor sampling and display update capabilities?

Issue
What is the granularity of the PM600 series processor sampling and display update capabilities?

Product Line
PM600 series meter

Cause
Customer would like to know sampling rate of PM600 meter series and how often does it update the display.

Environment
Configuration of PM600 series meter

Resolution
The Power Meter samples 64 datapoints per cycle every cycle. The display updates every 80ms. Alarms are checked every 500ms on the PM650.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: