Søg i ofte stillede spørgsmål
Status Flags for data in ION EEM
Goals and Symptoms
Each row in the Datalog table in ION EEM has a status flag that indicates the current status of that data point, one of the most important uses for this flags are in Data Quality to indicate which data points are valid, invalid or any other attribute the data can have.
Facts and Changes
EEM 3.95, Status, flags, datalog
Causes and Fixes
Here is a list of the possible values the StatusFlagsBitField column can take and its meaning:
-
- 0 = unknown
- 1 = invalid (failed Data Quality check)
- 2 = valid (passed Data Quality check)
- 4 = locked
- 8 = edited
- 10 = override enabled
This flags can be useful for tweaking data for running Data Quality procedures however it might be risky to do so, it is advised that changing this flags is avoided when possible.
Legacy KB System (APS) Data: RESL201426 V1.0, Originally authored by GeVe on 02/24/2010, Last Edited by GeVe on 02/24/2010
Related ranges: EEM V3.95
Udgivet til:Schneider Electric Danmark
Se mere
Område:
Se mere
Område: