PM870: Waveform capture misses event of interest...
Issue
Customer reports that waveform captures completely miss the triggering event, such as the transition to an under-current or over-voltage condition.
Product Line
PM870
Environment
ION Setup
PM8 platform
Cause
The waveform was configured to trigger on a Standard alarm. On PM8 series devices, Standard alarms have a 1-second detection cycle (see PM8 user guide, page 74). This delay can result in the waveform trigger occurring up to 60 cycles late, causing the event of interest to be missed.
Resolution
Use a Disturbance alarm instead of a Standard alarm to trigger waveform captures. Disturbance alarms operate on a cycle-based delay (e.g., 20ms per cycle at 50 Hz), providing much faster detection.
Steps in ION Setup:
- Open Onboard Alarms/Events dialog.
- You will see four alarm types: Standard, Disturbance, Digital, and Boolean.
- Select Disturbance and click Edit.
- In the Disturbance Alarm Setup dialog:
- Note that the delay is measured in cycles, not seconds.
- Configure the alarm according to your preferences.
- Click OK to save.