MGE RASP; Panel wiring for APC Products with the AP9610 or AP9613 Relay cards
Issue:
MGE RASP; Panel wiring for APC Products with the AP9610 or AP9613 Relay cards

Product line:
MGE RASP Panel

Environment:
All models/ All serial numbers

Cause:
Instruction on MGE RASP (Remote Alarm Status Panel) Panel wiring for APC Products with the AP9610 or AP9613 Relay cards

Resolution:
MGE RASP Panel wiring for APC Products with the AP9610 or AP9613 Relay cards

Refer to attached file for more details.


Schneider Electric Danmark

Bilag
AP9613 Installation and Configuration.pdf [499.81 KB]
QRMI2674-00-MM60.pdf [277.83 KB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: