Is the DC bus plate for the size 10 ATV61/71 drive available as a repair part?
Issue:
Availability of DC bus plate for size 10 ATV61/71 drive.

Product Line:
ATV61, Altivar 61, ATV71, Altivar 71

Environment:
Frame size 10.  ATV61HD90M3X, ATV61HC13N4, ATV71HD75M3X, ATV71HC11N4

Cause:
None

Resolution:
Due to safety reasons, Schneider Electric does not offer the DC bus plates separately for the ATV61 or ATV71 drives.  Contact Schneider Electric Industrial Repair Services to have the drive sent in for repairs. ph 800-950-9550

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: