What Telefast base is used with the BMEAHI0812 HART module?
Issue:
Telefast base that is used with the BMEAHI0812 HART module
Product Line:
Telefast
Resolution:
The following Telefast base can be used with the BMEAHI0812 HART module:
ABE7CPA02
ABE7CPA03
ABE7CPA31
using the BMXFTA1522/3022 cable
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance: