What is the maximum input voltage for Accutech TM10 Field Unit?
Maximum input signal clamping occurs at approximately 10Vp-p. So, 10Vp-p is the maximum input voltage for the TM10 Field Unit.

Schneider Electric Danmark