Which ATS01 softstarters have soft stop capability?
Issue:
Customer is looking for a small HP softstart that can soft stop as well.

Product line:
ATS01, Altistart 01

Resolution:
ATS01N1xxxx models have Soft START only
ATS01N2xxxx models have Soft START and soft STOP
ATSU01N2xxxx models have Soft START and soft STOP

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: