In SoMove software is there a way to print or export adjusted parameters?
Issue:
In SoMove how do you only Print or Export to Excel the Modified Parameters?

Product Line:
Altivar Machine, Altivar Process

Environment:
SoMove

Cause:
How to Print or Export Modified parameters only

Resolution:
To Print or Export only those parameters.  You go to the Device Menu > Select Printable Area
somove screenshot
Then deselect (uncheck) all options but Modified.
somove
Then Select the Printer icon
d
Or go to File and Print.
s

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: