Søg i ofte stillede spørgsmål
Osisense XC - Datasheet of the adapted XCMD connection component ZCMC21T4SF
Attached the datasheet of adapted XCMD connection component ZCMC21T4SF, using a special cable halogen free for railway equipments, complying to EN 50306 and EN 45545 standards. This reference is available to order without any restriction. It can be associated to ZCMD21 body. It is not in stock, it is produced at order reception by the assembly plant.
Udgivet til:Schneider Electric Danmark
Bilag
Se mere
Se mere