What can cause an OPF1 fault code on an ATV320 Drive?

Article available in these languages: Czech

Issue:
OPF1 fault on ATV320 Drive.

Product Line:
ATV320

Environment:
All

Cause:
NA

Resolution:
This fault is triggered when the drive detects one of the motor phases has been lost (or has very low current).
Check the connection between the drive and motor.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: