What is the impedance of DC Choke used with the ATV630 or 930 drives?
Issue:
Is additional line reactor needed with the process drives?

Product Line:
Altivar 600
ATV630, ATV650
Altivar 900
ATV930, ATV950

Environment:
All

Resolution:
The internal DC chokes provide a impedance between about 2 and 3.5%, depending on the drive.
If higher total impedance is needed, then a line reactor can be added up to max 5% total impedance (built-in plus additional combined).

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: