Can the output current of an EVH2S22P04K EvLink Wall box charging station be permanently limited? If so, to what level?
EVH2S22P04K can permanently limit its output current/power.

To limit the power:
1. activate power limitation mode in the charging station setting (see page 1 of Attachment1)
2. connect input E6 to 230V (see page 2 of Attachment1). The maximum charging power is limited as long as on the E6 is 230V.

The EVH2S22P04K is 32A station, therefore the power can be limited to level 16A (see page 2 of Attachment1).

Schneider Electric Danmark

Bilag
Attachment1.pdf [252.18 KB]
Se mere
Produkt:
Se mere
Produkt: