How to connect 4203DR current sinking AOUT to PLC with current sinking AIN?

Article available in these languages: Japansk

AOUT on 4203 cannot be connected directly to AIN on the SP350 because both are current sinking type of I/O.
Drawing shown below describes how AOUT on 4203DR transmitter should be connected to AIN on SCADAPack 350 when I-I Isolator is used.
Jumper for analog input on SCADAPack 350 must be in the Current position.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: