PM5500 Datalog Export tool
PM5560 supports datalog export using web pages. Setting up device log exports using the webpages.

Onboard datalog can be exported through HTTP. You can set up the meter to export its logs to a web server, either on a schedule or manually.

Refer the tool attached and follow procedure for exporting the data to server.

Schneider Electric Danmark

Bilag
DeviceLogExporter-V2.zip [3.12 MB]
PM556x_devicelogexport verification.pdf [758.26 KB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: