ClearSCADA has several recommended operational limits. Passive deviation around below listed limits may result in system that is unstable, unreliable and may cause slow performance in ViewX. The recommended operational limits for ClearSCADA clients are:
These operational requirements are for ClearSCADA 2017 R3 and older. Please check ClearSCADA Help for more up to date information on operational requirements for ClearSCADA Client.
- Minimum ViewX to ClearSCADA server link bandwidth = 2 Mbit
- Maximum ViewX to ClearSCADA server link latency = 150 ms
- Minimum WebX client to WebX server link bandwidth = 1 Mbit
- Minimum Original WebX client to ClearSCADA server link bandwidth = 1 Mbit
These operational requirements are for ClearSCADA 2017 R3 and older. Please check ClearSCADA Help for more up to date information on operational requirements for ClearSCADA Client.
Udgivet til:Schneider Electric Danmark