Description:
A common problem in SCADAPack Workbench happens when trying to download a logic using a serial port. The problem is “Download failed for Device: SCADAPack300E: The target running on the device: SCADAPack300E is not alive….” as shown below.

What causes this problem may be one of the following:
Workaround:
A common problem in SCADAPack Workbench happens when trying to download a logic using a serial port. The problem is “Download failed for Device: SCADAPack300E: The target running on the device: SCADAPack300E is not alive….” as shown below.
What causes this problem may be one of the following:
- The SCADAPack RTU may be powered off
- RS232 to USB converter driver is not installed or installed unsuccessfully (it is recommended to use Schneider Converter “TSXCUSB232”)
- Incorrect serial cable used (it is recommended to use Schneider Serial Cable “TBUM297217”).
- Microsoft Windows serial com port you assigned for this connection is busy.
- The configured RTU serial port function has a wrong function – it shall be ISaGRAF
- Communication settings (Com Port, Baud rate, Parity)
Workaround:
- Make sure that the com port settings are the same in the computer and Workbench as shown in the following photos
- Check the serial port configuration in the SCADAPack E Configurator where you connect your serial cable as shown
Note: After downloading the configuration file to the RTU you have to read the configuration to make sure that the modifications you made has been downloaded to the RTU.
- Remove the front cover of the RTU and make sure that the jumper beside the serial port used for downloading the logic is on RS232 as shown
- You may also Increase the Connection Timeout in the SCADAPack Workbench as shown
Udgivet til:Schneider Electric Danmark