Is an auger a constant torque (Heavy Duty) or variable torque (Normal Duty) application?
Issue:
Auger distinction between constant or variable torque application

Product Line:
NA

Environment:
All

Cause:
NA

Resolution:
It is a constant torque load.
When selecting a drive for this application be sure to select one rated and sized for Heavy Duty application (at least 150% overcurrent capacity).

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: