How to Link a VIM (Voltage Interface Module) to one of our Avatars Loads in TeSys Island
Product Line:
Industrial Automation Control
Environment:
Motor Management Systems TeSys Island
Cause:
What´s the correct path to add a Voltage Interface Module on of my avatar Loads
Resolution:
Voltage Interface Modules will require to be added to a specific Load Avatar in order to be mapped on the TeSys Island topology, to add this module, the correct path will be to first add our Load , it can be a standard starter or a SIL starter:
We will need to add a LOAD to My Avatar
To load our VIM we will need to add the Load Energy Monitoring in our Avatar Parameters window
This will automatically add the Voltage Interface Module to our LOAD and will be added to the Avatar Topology: