What is the difference between EASYCAN and VARPLUS CAN Capacitor?
The difference between Varplus Can and EasyCan is that:
EasyCAN is suitable for installations having THDi <5% and THDu of <3% while VarPlus Can is intended for installations having THDi of less than 8% and THDu of less than 5%..
For more information, you can download our Power Factor Correction catalogue on our global website via the following direct link:
Udgivet til: Schneider Electric Danmark