Issue
PME Software does not appear in the list of programs under Control Panel
Product Line
PME8.x
PSE8.2
Environment
PME 8.x
PSE8.x
Cause
There maybe instance where one needs to trouble shoot and possibly uninstall PME, but the program does not appear in the list of programs to uninstall or modify.
Resolution
Check if this system has PSE8.x with Advanced Reporting Module. If you see the Advanced Reporting Module, then that corresponds to the PME software. PSE with Advanced Reporting Module is a bundle package that incorporates a Power Scada system with PME software. The PME software that you normally see such as Management Console, Designer is under the name of Advanced Reporting Module.
PME Software does not appear in the list of programs under Control Panel
Product Line
PME8.x
PSE8.2
Environment
PME 8.x
PSE8.x
Cause
There maybe instance where one needs to trouble shoot and possibly uninstall PME, but the program does not appear in the list of programs to uninstall or modify.
Resolution
Check if this system has PSE8.x with Advanced Reporting Module. If you see the Advanced Reporting Module, then that corresponds to the PME software. PSE with Advanced Reporting Module is a bundle package that incorporates a Power Scada system with PME software. The PME software that you normally see such as Management Console, Designer is under the name of Advanced Reporting Module.
Released for:Schneider Electric Egypt and North East Africa