Tuotemerkkimme

Tervetuloa Schneider Electricin verkkosivustolle

Tervetuloa sivustollemme.
		
Kuinka voimme auttaa sinua tänään?
Can an ATV212 drive's programming be saved to the HMI keypad (VW3A1101)?
Issue:
Can I store the ATV212 program in the HMI VW3A1101?

Product Line:
Altivar ATV212

Environment:
All model numbers, all serial numbers

Cause:
N/A

Resolution:
No, the ATV212's programming cannot be saved to any of the keypads available.

Programming can be saved by any of three methods:
- in the drive by setting parameter tYP = 7
- in the Multiloader tool
- by using SoMove software