Tuotemerkkimme

Tervetuloa Schneider Electricin verkkosivustolle

Tervetuloa sivustollemme.
		
Kuinka voimme auttaa sinua tänään?
Can Ecostruxure Control Expert (formally Unity Pro) connect to a PLC using a DNS name ?

Issue:
Questions on weather Ecostruxure Control Expert can use DNS names.

Product line:
All products that are supported in Ecostruxure Control Expert.

Environment:
Ecostruxure Control Expert

Resolution:
Yes, Unity can use a DNS name server entry to look-up a domain name for the numerical IP address of the PLC.