Tuotemerkkimme

Tervetuloa Schneider Electricin verkkosivustolle

Tervetuloa sivustollemme.
		
Kuinka voimme auttaa sinua tänään?
How do I bring my Concept variables into Vijeo Designer?
Issue
Need a method for importing Concept Programming software variables into Vijeo Designer.

Product line
Concept, Vijeo Designer

Resolution
  1. Export Concept variables to a TXT file.
  2. Rename from a TXT to a CCN file extension.
  3. In Vijeo Designer, Right-click on the variable section and select link variables.
  4. If changes are required, select Update variables.