Tuotemerkkimme

Tervetuloa Schneider Electricin verkkosivustolle

Tervetuloa sivustollemme.
		
Kuinka voimme auttaa sinua tänään?
What does error EC02 mean in a Quantum HE CPU ?
EC02 is a failure in the Quantum Operating System. The CPU has encountered a non-maskable interrupt and as a result halted.

One possible cause of the EC02 error is the firmware version on the 140CRP93x 00. To prevent a possible EC02 error during startup the CRP93x must
have firmware version 2.10 or higher.

If the EC02 error is repeatable the CPU should be exchanged.