Tuotemerkkimme

Tervetuloa Schneider Electricin verkkosivustolle

Tervetuloa sivustollemme.
		
Kuinka voimme auttaa sinua tänään?
What is the processor speed of an Intel® iCoreTM 3rd generation 827E low power which comes with the Panel PC Universal (HMIPUxxxxxxx)
Issue:
What is the processor speed of an Intel® iCoreTM 3rd generation 827E low power which comes with the Panel PC Universal (HMIPUxxxxxxx)

Product Line:
Panel PC Universal (HMIPUxxxxxxx)

Resolution:
Intel® iCoreTM 3rd generation 827E low power is a Celeron M 827E 1.4GHz processor.