Tuotemerkkimme

Tervetuloa Schneider Electricin verkkosivustolle

Tervetuloa sivustollemme.
		
Kuinka voimme auttaa sinua tänään?
Why does the speed increase so slow when using the ATV312 jog dial in local control?
Issue:
Speed increasing slow when using the ATV312 jog dial in local control.

Product Line:
ATV312

Environment:
All models and serial numbers

Cause:
None

Resolution:
Turning the jog dial slowly causes a minute change in the speed increments. If the jog dial is continued to be turned quickly, the speed increment increases.