Tuotemerkkimme

Tervetuloa Schneider Electricin verkkosivustolle

Tervetuloa sivustollemme.
		
Kuinka voimme auttaa sinua tänään?
It is possible to use HMI as Remote Gateway for OPC Server access to connect PLCs on Remote side?
Until SoMachine V3.1 / VJD 6.1 it was possible to connect Remote PLC to an OPC Server by using the remote HMI as Gateway.

With VJD 6.2 SP 2.x this was not any more working, because of an issue inside the VJD runtime.

But in VJD 6.2 SP3 it is fixed and can be used again.


Schneider Electric Suomi

Liitteet
faq_frank.png [24.14 KB]