Tuotemerkkimme

Tervetuloa Schneider Electricin verkkosivustolle

Tervetuloa sivustollemme.
		
Kuinka voimme auttaa sinua tänään?
What can cause an ECF [Encoder Coupling] Fault on an ATV340 drive?
Issue:
Customer is experiencing an ECF [Encoder Coupling] Fault on their ATV340 drive.

Product Line:
ATV340

Environment:
Encoder function is being used.

Cause:
The mechanical coupling of the encoder is broken.

Resolution:
Verify the mechanical coupling of the encoder.