Tuotemerkkimme

Tervetuloa Schneider Electricin verkkosivustolle

Tervetuloa sivustollemme.
		
Kuinka voimme auttaa sinua tänään?
Why the BMXAMI0810 only reports MOD_ERROR in the IODDT?
  1. Issue
Why the BMXAMI0810 only reports MOD_ERROR in the IODDT T_GEN_MOD?
  1. Environment
N/A
  1. Resolution
When any channel comes across brokenWireupperOvrlowerOvspiErroror HARDWARE_SELF_TEST_FAULT, the MOD_ERROR will be activated. In special when the channel
has problems, the CH_ERROR will be activated also.
If there is only MOD_ERROR in the IODDT, customer has to verify the upper overflow or lower overflow.