{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do I need to Earth my ASi Power supply?
For the following units it is recommended to earth the ASi system at the power supply:
  • ASIABLB300*
  • ASIABLM3024

For the following units it is mandatory, this is because the unit is designed to detect Earth faults:
  • ASIABLD300*

Earthing should be to the GND terminal. The GND terminal is internally linked and it is therefore only necessary to connect to earth at one point.

Please note that this range was made obsolete in 2018 without replacement. Schneider Electric UK no longer supports the ASi system.

Schneider Electric Ireland