How to read open channel/wire in unity pro for 140ACO13000.
Open circuit in 4 ... 20 mA mode. The open channel/broken wire is indicated through the red channel LED and is also reported back to the controller in the I/O Map status byte .Refer the attached document(Quantum IO module status Byte configuration.pdf) to understand how to configure the I/O Map Status in Unity pro.