It is not possible to import an asc file which was created with the menu item "project with used DFBs (Re-Connect to Equal)". The Concept Converter allows only asc files which are created like described in the Unity online help. While exporting the application from Concept, do not use the export range "Project with used DFBs(Re-connect to Equal)".