本日はどのようなご用件でしょうか?

Video: 無線スイッチ/ ZBRN1のIPアドレスはどのように設定しますか?

⚠ CAUTION ⚠

The information provided in this FAQ being considered as confidential content, as it can be exclusively used internally.

This flag has been added automatically when the article is published with internal visibility only.

ZBRN1の本体上で設定します。
設定方法を下記の動画で説明します。