What is typical life expectancy of a low voltage dry type Distribution Transformer?
Issue:
Low Voltage Dry Type Distribution Transformers have a finite potential lifetime
Product Line:
Low Voltage Transformers
Environment:
Applies to Low Voltage Dry Type Distribution Transformers by SquareD/Schneider Electric
Cause:
Lifetime estimates can be affected by many factors
Resolution:
The life expectancy under various loading conditions of a low voltage dry type Distribution Transformer can be calculated using ANSI Standard C57.12.96 (Schneider Electric cannot supply a copy of this standard as it is copyrighted material.)
Industry experience has demonstrated that a low voltage dry type Distribution Transfomer with typical loading as found in the majority of installations will satisfactorily serve 20 to 30 years or even longer.
Publicado para: Schneider Electric Mexico