Is ''trapeze'' mounting a low voltage dry type distribution transformer the same as using a Square D ceiling mounting bracket with customer supplied hardware (threaded rod, springs, washers, nuts...)?
''Trapeze mounting'' definition.
Product Line:
Transformers
Environment:
Class 4800 type transformers
Resolution:
Yes, they are commonly considered to be equivalent. For absolute clarification of the mounting style desired by the specifying engineer it is recommended that you send a RFI (request for information) to the specifier.